Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What are inputs impedance values for some X80 analog inputs module.
Some clarifications are requested for information related in documentation concerning X80 analogues modules.

Modification related to products BMX AMI 0810, BMX AMI 0810H, BMX AMI 0410, BMX AMI 0410H
Please do NOT read: 250 ohm internally protected resistors
Please read: The internal protection resistor has a typical impedance of 25 Ω (min 3.6 Ω and max 50 Ω),
The precision of the protection resistor does not impact the measured value.


Modification related to product BMEAHI0812
Please read: The internal protection resistor has a typical impedance of 25 Ω (min 3.6 Ω and max 50 Ω),
The precision of the protection resistor does not impact the measured value.
Modification related to products BMX AMI 0800, BMX AMI 0800H, BMX AMI 0600, BMX AMI 0600H
Please do NOT read: 250 ohm internally protected resistors

Schneider Electric Saudi Arabia