{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to clean a Condensate drain line on an ACSC100 unit
Issue:
How to clean a Condensate drain on a ACSC100 unit..

Product line:
ACSC100 and ACSC101

Environment:
All Serial Numbers...

Cause:
Clog due to debris or sediment

Resolution:
See Attached video

This video will show you how to remove and clean clogged drain lines and clogged condensate pumps on an ACSC100 unit.  Ensue the unit is powered off then unplug the unit from power.  When using compressed air please ensure safety glasses are used.  Will also need to create a seal to slightly pressurize the line.

Schneider Electric Saudi Arabia