Search FAQs
What replacement enclosures are available for the 8903 Type L and LX lighting contactors?
Issue:
Enclosures for Class 8903 Type L and LX lighting contactor.
Product Line:
8903 NEMA Lighting Contactors
Environment:
NEMA Contactors and Starters
Resolution:
Options include the following,
NEMA 1 - Surface Mount Enclosure: 9991LXG1
NEMA 3R - Enclosure: 9991SDH1
NEMA 4 - Standard Enclosure: 9991SDW1
NEMA 4 - With 2 Cover Mtd. Closing Plates: 9991SDW11
NEMA 4X - Glass Polyester Enclosure: 9991SDW20
NEMA 12 - Enclosure: 9991SDA11
NEMA 1 Flush Mount Parts:
Cover: 9991SDF13
Mounting Strap: 9991SDF2
Pull Box: 9991SDF1
Oversized enclosures (where cover mounted controls are needed):
NEMA 1: 9991SDG3
NEMA 4: 9991SDW3
NEMA 12: 9991SDA3
Enclosures for Class 8903 Type L and LX lighting contactor.
Product Line:
8903 NEMA Lighting Contactors
Environment:
NEMA Contactors and Starters
Resolution:
Options include the following,
NEMA 1 - Surface Mount Enclosure: 9991LXG1
NEMA 3R - Enclosure: 9991SDH1
NEMA 4 - Standard Enclosure: 9991SDW1
NEMA 4 - With 2 Cover Mtd. Closing Plates: 9991SDW11
NEMA 4X - Glass Polyester Enclosure: 9991SDW20
NEMA 12 - Enclosure: 9991SDA11
NEMA 1 Flush Mount Parts:
Cover: 9991SDF13
Mounting Strap: 9991SDF2
Pull Box: 9991SDF1
Oversized enclosures (where cover mounted controls are needed):
NEMA 1: 9991SDG3
NEMA 4: 9991SDW3
NEMA 12: 9991SDA3
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: