Issue
How to access the SNMP value from OPC Server in ConneXium Network Manager using an OPC client.
Product Line
OFS, ConneXium Network Manager.
Environment
Windows 10
Resolution
The following steps can be used to access the SNMP values store in the OPC server that gets installed with
ConneXium Network Manager from an OPC client (e.g., OFS Testing Client, etc.)




How to access the SNMP value from OPC Server in ConneXium Network Manager using an OPC client.
Product Line
OFS, ConneXium Network Manager.
Environment
Windows 10
Resolution
The following steps can be used to access the SNMP values store in the OPC server that gets installed with
ConneXium Network Manager from an OPC client (e.g., OFS Testing Client, etc.)
- Start the 'OFS Testing Client'.:
- Select the 'Schneider Electric ConneXium Network Manager OPC Server'.
- Click on OK.
- Click on 'Gourp\New Group'.
- Click on OK.
- Select 'Item\New' to open the 'Additem' window.
- Expand the Add item tree to select the respective OPC tag.
- Select the value that you want to see.
- Click on OK.
- A window will appear to show the SNMP value.
Released for:Schneider Electric Saudi Arabia