{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the RS485 communication cable part number to go from an M221 to an HMISTU?

There are two cable part numbers that can be used to communicate between the M221 and HMISTU over RS485 MB serial.
- XBTZ9980 (2 RJ45 connectors)
- VW3A8306R** (2 RJ45 connectors)

- ** = length of cable (03 = 0.3M, 10 = 1M, 30 = 3M)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: