{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I get the Magelis HMI to communicate to the Unity Pro Simulator?
Issue
Can I get a Magelis or Harmony HMI to communicate to the Unity Pro or EcoStruxure Control Expert Simulator?

Product Line
Harmony / Magelis XBTGC/GH/GK/GT, HMIGTO/GTU/STO/STU, iPCs, Panel PC, Box PC, Unity Pro, EcoStruxure Control Expert

Environment
Physical HMI Communication with Simulated PLC

Resolution
Yes, it is possible for the Harmony or Magelis HMI communicate to an EcoStruxure Control Expert or Unity Pro simulator.  Make sure in the Modbus/TCP driver in Vijeo Designer is used.  The IP address of the Equipment is the IP address of the PC that is running the EcoStruxure Control Expert or Unity Pro Simulator. The PC will need to open TCP Port 502.

If the Vijeo Designer Simulation is on the same PC as the PLC Simulation, the IP Address needed is 127.0.0.1 (the local host).

Schneider Electric Saudi Arabia