{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What terminals can the speed pot be wired to on the Altivar ATV61 and ATV71 drives?
Issue:
Terminals to connect Speed Potentiometer on ATV61/71 Drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to know where the Pot can be wired on the ATV61 or ATv71 drive.

Resolution:
The Pot will have 3 terminals  The center terminal is the wiper it is wired to AI1+
1st leg is wired to +10vdc
3rd leg is wired to com that is jumpered to AI-

Schneider Electric Saudi Arabia