{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to compare two programs / projects in SoMachine versions 4.1, 4.2 or 4.3?
In SoMachine versions 4.1, 4.2 or 4.3 you can use the command located under the Logic Builder / Project / Compare to compare the actual project with another one (reference project). The reference project and the compare options are specified in the Project Compare dialog box, which opens, when the command is executed.

Schneider Electric Saudi Arabia