{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
Issue:
Customers want to know if there is flexibility in installing vertical cable managers, or where to mount the 0U accessory rails.

Product Line:
NetShelter SX Vertical Cable Management

Environment:
All versions and serial ranges.

Cause:
Owner's Manuals show cable managers and 0U accessory rails installed in specific areas of the cabinet.

Resolution:
The 0U accessory rails that come preinstalled in the rear of the SX cabinet can be moved to the front of the cabinet. Anything that attaches to the accessory rail can also be mounted in the front of the cabinet such as cable management or PDUs.


Schneider Electric Saudi Arabia