{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Power Array/Masterframe System Fan Replacement

Issue
The need to replace the system fans on the Power Array/Masterframe

Product Line
SYMINIF, SYMINIF-PD, SYMSTRF, SYMSTRF-PD

Resolution
The system fans on a Power Array is not hot-swappable. A complete power off of the system must be done to replace the system fan.

1. Set the System enable Switch to Standby
2. Set the Input Circuit Breaker to Standby
3. Disconnect the Battery Modules
4. Disconnect external Battery Cabinet (if provided)
5. Disconnect Mains/Branch Circuit

Remove all 4 screws holding the fan chassis in place



Carefully pull fan out to access the 6 pin connector. Disconnect the fan from connector.



Connect new fan to 6 pin connector and reattach fan chassis using previous 4 screws.



Schneider Electric Saudi Arabia