What can I do if the PLC TM221 reboots continuously after an update with firmware 1.3.2.1 SP1?
Article available in these languages:Japanese
This issue can be solved by downloading any application in the PLC TM221 via USB in powerless mode (no power supply connected). After that, the issue will not appear anymore.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Modicon M221
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.