{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a line reactor be added to the line side of an ATV212 drive?
Issue:
Line reactor on line side of ATV212.

Product Line:
ATV212

Environment:
All products of ATV212

Cause:
N/A

Resolution:
In most cases, the ATV212 drive does not need a line reactor due to the low harmonic mitigation designed into the drive.  If the application determines that one is needed, a 1.5% maximum Line Reactor is recommended.

Schneider Electric Saudi Arabia