{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SPM Web Application Diagrams Display the Message "The stylesheet is too complex"
Issue
Browsing the Diagram Application in Web applications displays the error message "The stylesheet is too complex"

Product
StruxureWare Power monitoring (SPM) 7.0.1

Environment
.Net Framework 4.5 and later

Cause
With changes to the .Net Framework in 4.5, if a diagram has more than 170 status objects on a single page this error message is displayed.

Resolution
SPM 7 does not officially support .Net 4.5. This issue does not occur if using .Net 4.0 or later versions of Software.

Schneider Electric Saudi Arabia