Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How do you activate or deactivate the Front USB port on a HMIDT732 when connected to a HMIG5U?
To activate or deactivate the Front USB port on the HMIDT732 panel when connected to a HMIG5U, goto the Windows Start Menu and launch the application Front USB Setting. The application will provide two options, enable or disable. Once a setting change has been made, the HMIG5U will reboot.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: