{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Part number TSXP57252 has been obsoleted, what is it's replacement?
Issue:
Part number TSXP57252 has been obsoleted, what is it's replacement?

Product Line:
Modicon TSX Premium, TSXP57252, TSXP57253M


Resolution:
The original suggested replacement for the TSXP57252 is TSXP57253M.  Only difference is that TSXP57253M is a double wide versus the TSXP57252 is single wide.  The double wide means that the controller will occupy 2 slots on the backplane.  So, if the customer does not have any empty slots available.  They will need to get a bigger backplane.

However, the Premium PLC Family has been discontinued since 2018, a full upgrade to a newer family of PLC would be required.
Please search for "Unity M580 Application Converter" also known as UMAC. This tool helps migrating from older PLCs to the latest Modicon M580 family.

Schneider Electric Saudi Arabia