Text on screen vs numeric. Many of customers require them to identify the crane as (Axle Crane or Rim Crane or Transfer Crane) very few us a number to identify the crane. So could text be possible?
We have not implemented an alphanumeric identification today. If this is a strong request, we have to made a study. It is also necessary to keep in mind that the size of the display will limit the number of characters and the the freedom for names to be displayed is limited.
Released for: Schneider Electric Saudi Arabia
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.