Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
If the operator use eXLhoist in a driver room (like use joystick), and the distance is nearly 15 meters, is this ok to use ?
We made some tests here and 15 meters should be not a problem. Anyway it depends on the material of the separation between the driver room and the Base. The external antenna can be used in order to reassure the customer.

Schneider Electric Saudi Arabia