What is the reaction of the product when devices as WIFI are emitting under 2,4GHz
Because with the frequency hopping given by our protocol we avoid there pollution. The complete design of eXLhoist was done with a Wi-Fi station at 1,5 m from the systems. No perturbation was identified.
Released for:Schneider Electric Saudi Arabia
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.