{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the dimensions changing if we change from copper to Aluminium or vice versa for Oil Distribution Transformers?
Yes,the dimensions are changing if we change from copper to Aluminium or vice versa. The overall dimensions will be affected in case we change the winding material. Usually for the same electrical characteristics (same power rating, same voltage ratio, same impedance, same loss values) the transformer footprint will be bigger if we change the winding material from copper and aluminium for Oil Distribution Transformers.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.