{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers for the RJ45 Modbus cables for Schneider drives and soft starters?
VW3A8306R03 -  0.3 meter length cable / 1 foot
VW3A8306R10 - 1 meter length cable / 3 feet
VW3A8306R30 - 3 meter length cable / 9 feet

NOTE:  These cables will not work for connecting a remote mounted keypad for the drives/softstarts.
The best cables for remote keypad connections are:
VW3A1104R10 - 1 meter long / 3 feet
VW3A1104R30 - 3 meters long / 9 feet
VW3A1104R50 - 5 meters long / 15 feet
VW3A1104R100 - 10 meters long / 30 feet

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: