Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the derating when Prisma system is installed in altitude?
The standard 61439-2 is valid for an altitude up to 2000m. With altitude the atmosphere is modified, cooling efficiency and dielectric properties are impacted.
When installed above 2000m altitude, Prisma P, G and Linergy BS, LGY, LGYE must be derated for the voltage Ui and current.

- The most impact is on voltage (Ui,Ue). As Ui may decrease significantly with the altitude, it must stay valid for the real Ue.
- About the current, the derating should be applied as per the devices altitude derating. (ie: breakers NSX, NW . . .). these deratings are generally given in devices catalogues and may change, depending the ranges.

For Prisma range of products, deratings are:
Altitude0-2000 mup to 3000 mUp to 4000 mUp to 5000 m
Voltages Ui           k=10.880.780.68
Current                  k=As per installed devices altitude derating

More information on the physical phenomena is available in IEC60664 §5.1.2, and “Paschen law” (atmospheric characteristics modified with altitude)

Schneider Electric Saudi Arabia

What is the derating when Prisma system is installed in altitude?
The standard 61439-2 is valid for an altitude up to 2000m. With altitude the atmosphere is modified, cooling efficiency and dielectric properties are impacted.
When installed above 2000m altitude, Prisma P, G and Linergy BS, LGY, LGYE must be derated for the voltage Ui and current.

- The most impact is on voltage (Ui,Ue). As Ui may decrease significantly with the altitude, it must stay valid for the real Ue.
- About the current, the derating should be applied as per the devices altitude derating. (ie: breakers NSX, NW . . .). these deratings are generally given in devices catalogues and may change, depending the ranges.

For Prisma range of products, deratings are:
 
Altitude0-2000 mup to 3000 mUp to 4000 mUp to 5000 m
Voltages Ui           k=10.880.780.68
Current                  k=As per installed devices altitude derating
 
More information on the physical phenomena is available in IEC60664 §5.1.2, and “Paschen law” (atmospheric characteristics modified with altitude)

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.