Search FAQs
Which brackets should be used to install a NetShelter SX into a IBC High Seismic Area?
Issue:
There is need for a NetShelter SX mounting bracket that's rated for installation in a IBC High Seismic Area.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
A NetShelter SX cabinet needs to be installed into an IBC High Seismic Area.
Resolution:
AR7701A-S is rated for NetShelter SX cabinets to be mounted in an IBC High Seismic Area.
AR7701A-S replaces both AR7701-S and AR7701 in IBC High Seismic Area installations.
Do not use the AR7701 in an IBC High Seismic Area installations of NetShelter SX cabinets.
For cabinets installed in an IBC Low Seismic Area or Moderate Seismic Area the included pallet bracket or AR7701 can be used to mount the cabinet.
There is need for a NetShelter SX mounting bracket that's rated for installation in a IBC High Seismic Area.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
A NetShelter SX cabinet needs to be installed into an IBC High Seismic Area.
Resolution:
AR7701A-S is rated for NetShelter SX cabinets to be mounted in an IBC High Seismic Area.
AR7701A-S replaces both AR7701-S and AR7701 in IBC High Seismic Area installations.
Do not use the AR7701 in an IBC High Seismic Area installations of NetShelter SX cabinets.
For cabinets installed in an IBC Low Seismic Area or Moderate Seismic Area the included pallet bracket or AR7701 can be used to mount the cabinet.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: