{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for the 8839 58M series enclosed drive?
Issue:
Replacement for the 8839 58M series enclosed drive

Product Line:
8839 58M enclosed custom drives

Environment:
8839 58M enclosed custom only

Cause:
Needs a replacement for the 58M drives

Resolution:
Consider the ATV660 product line as a possible replacement for the old 58M drives.  See attachments to break down the 58M part number and review the ATV660 specifications.  The ATV660 part number can be built in the product selector.  Contact your local distributor for assistance.

Schneider Electric Saudi Arabia

Attachment(s)
NHA91297_02 ATV660.pdf [7.26 MB]
8839 58M breakdown.pdf [35.96 KB]