{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to download the boot application onto the M238?
Issue:
How to download the boot application onto the M238?

Product Line:
Somachine, M238, boot application

Environment:


Cause:


Resolution:
There are two ways of getting the boot application onto the M238:
1 - When online to the controller, put it to STOP, then run the Boot Application
2 - Select Multiple Download and check the bullet point for "Always perform a full download".

Schneider Electric Saudi Arabia