{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to update M580 application from CPUv1.xx to v2.0?
In Unity v10's release notes:
(**) A M580 application with CPU V1.1x (developed with Unity Pro V8.0 or 8.1, or 10.0)  cannot be updated to CPU V2.0 : due to compatibility issues, the “Change CPU” option is not allowed. The proposed solution is to export/import variables and program into a new application.

Schneider Electric Saudi Arabia