{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an E21 fault on the Altivar ATV21 and ATV212 drives?
Issue:
E21 fault code on ATV21 and ATV212

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Drive powers up with an E21 CPU is failing

Resolution:
The E21 is a CPU error 2 fault.   If you power cycle and the fault does not clear the drive will need to be replaced.

Schneider Electric Saudi Arabia