Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What adjustments can be made to the ATS48 soft starter if max starting torque is needed?
Issue:
Adjustments that can be made to the ATS48 soft starter, if the motor is stuck and max starting torque is needed?

Product Line:
Altistart, Altistart 48

Environment:
All

Cause:
Motor is stuck, or conveyor or grain elevator is loaded down. Need to increase starting torque to get the load moving

Resolution:
If the motor is stuck, or if more torque is needed to help move the load on start up, try adjusting the following parameters:

DRC menu make sure your Torque control CLP is set to Yes.
SET menu set the t90 or Initial starting torque from 20% to 100% depending on what amount of torque is needed to start.
ILT= current limit try increasing 400% to 700%
tHP= Motor thermal protection set to class 20.

Once the motor breaks loose you can set all of the above parameters back to the original settings.
These settings can be left this way if desired, depending on customer's preference. However, be aware that maximum torque is being applied to your machines, and equipment damage may incur in situations where maximum torque isn't needed.

Schneider Electric Saudi Arabia

Attachment(s)
ATS48 Y Range basic.pdf [1.78 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.