{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up the analog output or AO1 on the ATV61 and ATV71 drives?

Article available in these languages: Spanish

Issue:
Setup for analog output or AO1 on ATV61 & ATV71.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to set up the analog output for frequency with min 4mA and max 20mA.

Resolution:
Programming
Menu 1.5 I/O or inputs and outputs
AO1 assignment
Assign to motor frequency
Type: current
Min 4mA Max 20mA

Schneider Electric Saudi Arabia