Search FAQs
How many XVGU Tower Lights can be connected to a Magelis HMI?
Issue:
It is not possible to connect more than one XVGU to a Magelis HMI.
Product Ranges:
XBTGT, XBTGK, HMISTU, HMISTO, HMIGTO, HMIGTU, iPC.
Resolution:
Vijeo Designer runtime only supports 1 XVGU connection at a time. The HMI is only able to detect one device of the same USB device type at a time.
It is not possible to connect more than one XVGU to a Magelis HMI.
Product Ranges:
XBTGT, XBTGK, HMISTU, HMISTO, HMIGTO, HMIGTU, iPC.
Resolution:
Vijeo Designer runtime only supports 1 XVGU connection at a time. The HMI is only able to detect one device of the same USB device type at a time.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: