{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Latest firmware version for the energy server COM'X 510 (Version 6.6.5)
Issue
What is the latest firmware version for the Energy Server Com'X 510 ?
Product Line
COM'X 510
EBX 510

Environment
COM'X 510

Cause
The new firmware upgrade is needed
Resolution
As of 05/07/2024, the latest version of firmware for COM'X 510 is 6.6.5 and can be downloaded from the link below:

EBX510 - ComX 510 - energy server - UL - SDRAM4 Go | Schneider Electric USA

Instructions for upgrading the firmware can be found from FAQ: How to upgrade the firmware on Energy Server COM'X 200, 210 or 510 via the web page or USB port? | Schneider Electric USA

Schneider Electric Saudi Arabia