Search FAQs
Which cable reference can we use between TM3XTRA1 (TM3 bus extension transmitter module) and TM3XREC1 (extension receiver module)
The extension receiver module TM3XREC1 can be at maximum distance of 5 meters from the TM3XTRA1
The Catalog recommend to use the references VDIP1845460xx;
VDIP184546005 (0.5 m)
VDIP184546010 (1.0 m)
VDIP184546020 (2.0 m)
VDIP184546030 (3.0 m)
VDIP184546050 (5.0 m)
But as these references does not meet the UL requirements , for US market machines installation needs it’s advised to use 2 other references:
490NTW00002U (2.0 m)
490NTW00005U (5.0 m)
which are UL rated
The Catalog recommend to use the references VDIP1845460xx;
VDIP184546005 (0.5 m)
VDIP184546010 (1.0 m)
VDIP184546020 (2.0 m)
VDIP184546030 (3.0 m)
VDIP184546050 (5.0 m)
But as these references does not meet the UL requirements , for US market machines installation needs it’s advised to use 2 other references:
490NTW00002U (2.0 m)
490NTW00005U (5.0 m)
which are UL rated
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: