{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to use PSE to control PM5350’DO via PwrModubs protocol
1. First using PM5350 to control we need to write 3 register together. If we want to send command to DO1 to  we need to write 5250=6003,5251=0 and 5252=1 and send  the frame  like :01 10 14 81 00 03 06 17 73 00 00 00 01 XX XX. (XX XX is for CRC).

2. We can use the block writes to write multiple registers. By using fixed block writes follow the format below:
Fixed block writes have the following format:
T:BWF;[D:{B|C|M|P};]S:<start_register>,<values>
where
B, C, M, or P are applicable only to Micrologic devices (otherwise the D: section
is omitted) and is the module (manager) identifier (Circuit Breaker, Chassis,
Metering, Protection).
<start_register> is the first register number for a contiguous block of registers.
<values> is a comma-separated list of up to 10 values that will be written to the
registers starting from <start_register>.
For PM5350 control tag looks like T:BWF;S:5250,6003,0,1 and this tag must be DIGITAL. By setting this tag to 1 to make it works.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.