Search FAQs
Compatibility & Inter-Operability between Vijeo citect, Vijeo Historian, Ampla and windows O.S and Office platforms and connectors.
Check attached PDF for compatibility and inter-operability.
Compatibility Matrix
1 Vijeo Citect V7.30 Service Pack 1 is the minimum requirement to be compatible with Windows 8 and Windows Server 2012. Windows 8.1 is not confirmed at this time.
5 Vijeo Citect V7.20 Service Pack 5 is the minimum requirement to be compatible with Windows 8.1 and Windows Server 2012 R2.
3 Vijeo Citect V7.10 Service Pack 3 is the minimum requirement to be compatible with Windows 7.
+ Not supported as a database for Inventory. Other modules are supported.
^ Windows 8.1 is not confirmed at this time
# Ampla supports the operating system on the client side only.
♦ Ampla 2014 and 2013 Server is compatible with the 64 bit version only. The client supports 32 and 64 bit.
Software is compatible with the 32 bit version only
▶ Server only
∞ Client only
Inter-operability
*Software is installed as part of PlantStruxure PES suite # Software is compatible via an OPC DA Connector only
Compatibility Matrix
1 Vijeo Citect V7.30 Service Pack 1 is the minimum requirement to be compatible with Windows 8 and Windows Server 2012. Windows 8.1 is not confirmed at this time.
5 Vijeo Citect V7.20 Service Pack 5 is the minimum requirement to be compatible with Windows 8.1 and Windows Server 2012 R2.
3 Vijeo Citect V7.10 Service Pack 3 is the minimum requirement to be compatible with Windows 7.
+ Not supported as a database for Inventory. Other modules are supported.
^ Windows 8.1 is not confirmed at this time
# Ampla supports the operating system on the client side only.
♦ Ampla 2014 and 2013 Server is compatible with the 64 bit version only. The client supports 32 and 64 bit.
Software is compatible with the 32 bit version only
▶ Server only
∞ Client only
Inter-operability
*Software is installed as part of PlantStruxure PES suite # Software is compatible via an OPC DA Connector only
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: