{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to display the motor speed in RPM, on the screen of an ATV61/71?
Issue:
Need to display the motor speed in RPM on ATV61/71

Product Line:
Variable Frequency Drives

Environment:
Applies to all Altivar 61 and Altivar 71 with a graphical display VW3A1101

Cause:
Customer wants to display the motor speed in RPM on the screen

Resolution:
There are two methods and areas on the screen that you can display the motor rpm on

Option 1: This will display the motor rpm on the top parameter bar of the screen
- Go to menu 6 Monitoring Config
- Go to menu 6.1 Parameter bar select
- Select the parameter you want to show such as motor speed


Option 2: This will display the motor rpm on the main screen in the middle in big numbers
- Go to menu 6 Monitoring Config
- Go to menu 6.2 Monitor screen type
- Enter into Parameter selection
- Select the parameter you want to show such as the motor speed

Schneider Electric Saudi Arabia