{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
TM3SAC5R safety module wired for the E-Stop but when E-Stop is activated K1 closes but not K2. K2 would just flicker and does not stay closed, why?
Issue:
TM3SAC5R safety module wired for the E-Stop but when E-Stop is activated K1 closes but not K2.  K2 would just flicker and does not stay closed, why?

Product Line:
TM3 Safety, TM3SAC5R

Resolution:
Ensure activation of the SA_ENABLE in the EcoStruxure Machine Expert-Basic / SoMachine Basic Program.
This must do via programming code or via a watch window.

Schneider Electric Saudi Arabia