{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to set the date and time on all Sepam series 10 versions?
Only Sepam 10A has the option of time and date stamping as it is the only version that can have time-tagged event recording that is why it is the only version where it is possible to set the date and time. Sepam 10 version B and N do not have this time-tagged recording option thus they do not have a real-time clock.

AEDL3

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.