{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
MiCOM relays. Specific timers related to the user interface in the MiCOM Px2 relays.
Follwowing timers are fixed in the Px2 relays.
  • LED refresh time is 500 ms
  • LCD refresh time is 1 s
  • The password confirm info display time delay is 2 s
  • Programming mode timer after login to the front panel is 5 min. During this time the relay will not accept to change any settings from remote. It is considered as 5 min of inactivity.

Schneider Electric Saudi Arabia