Search FAQs
What is the difference between CAD32FD and CAD323FD? Data sheets of both doesn't mention any difference?
The technical specification of the both of the Tesys D control relay's are same except the below two differences.
1. CAD32FD is provided with Screw Clamp Terminals for size 1...4 mm², but the CAD323FD is provided with Spring Terminals for size 1...2.5 mm²
2. The hight of CAD32FD is 77mm and the hight of CAD323FD is 99mm.
All other specifications are same for both relays.
1. CAD32FD is provided with Screw Clamp Terminals for size 1...4 mm², but the CAD323FD is provided with Spring Terminals for size 1...2.5 mm²
2. The hight of CAD32FD is 77mm and the hight of CAD323FD is 99mm.
All other specifications are same for both relays.
Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Range:
Explore more
Category:
Range: