{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you please provide us the type 2 coordination table for starter with Class 20 LRD over load relay?
​There is no separate type 2 coordination available for starter with Class 20 LRD over load relay.

But please refer the attached technical complementary guide for type 2 co-coordination, it is clearly mentioned that "for motors with long starting times, the class 10 or 10 A thermal relays must be replaced with class 20 thermal relays as indicated in the correspondence table opposite (for type 1 and type 2 coordination)".

Hence you can use the same co-ordination table by replacing the relay as indicated in correspondence table in given attachment.

Schneider Electric Saudi Arabia

Attachment(s)
Technical complementary guide - Type 2 co-ordination.pdf [791.24 KB]