{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If the BME rack can be used as an extension rack in M580 system?
In future Unity v11, the BME rack will possible to be configured as an extension rack, but only X-bus is available.

Schneider Electric Saudi Arabia