{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can we get spare parts for removable terminal blocks of TM3 modules?

Article available in these languages: Japanese

For TM3 modules using terminal blocks with pitch 5.08 mm, no spare part for the terminal blocks is available.
It concerns the following TM3 module references: TM3DI8x, TM3DQ8x, TM3DM8x, TM3AI2Hx, TM3AQ2x, TM3AQ4x and TM3TM3x.
For those references, a complete TM3 module has to be ordered again in case of connector loss/damaged.

Spare parts references are available for TM3 modules having terminal blocks with pitch 3.81 mm only:
  • TMAT2MSET: including a set of terminal blocks 10 ways and 11 ways with screw terminals
  • TMAT2MSETG: including a set of terminal blocks 10 ways and 11 ways with spring terminals

Schneider Electric Saudi Arabia