{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
VIP13 relay - is there a replacement for the legacy VIP13 protection relay?
Please see the files attached to this FAQ for more information.

The VIP13 has been discontinued in 2004 and can be replaced by the VIP300P, which is still available through Schneider distribution centers.

The 2 products use the same current sensors: CSa for 630A and CSb for 1250A.

The cases have different form factors so an adaptation kit is needed. This kit, designed by Ecofit activity, is not available anymore.  However it's a simple plate so it should not be difficult for a system integrator also attached a view of VIP300P front panel and all the info I found on VIP13 / 300P.  Note: the VIP range is designed by AED based on an MVS specification and it is sold by MVS (not AED, except for spare parts)

Schneider Electric Saudi Arabia

Attachment(s)
Case_21539154_VIP13_VIP300_DMO.zip [1.16 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.