{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to wire an ATV61 or ATV71 for 2 wire control?

Issue:
Wiring an ATV61/71 for 2 wire control.

Product Line:
Altivar 61, ATV61

Environment:
All

Cause:
N/A

Resolution:
Wire connections will be between +24 and LI1.  This is assuming the drive's +24 source will be used.
This is maintained contact setup.

Schneider Electric Saudi Arabia