{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What causes a TNF on an ATV61 or ATV71 drives?

Article available in these languages: Turkish

Issue:
TNF on the ATV61/71 drives

Product Line:
Altivar 61, Altivar 71

Environment:
All

Cause:
N/A

Resolution:
Check that the motor is connected to the drive.
If an output contactor is used, close it during auto tuning.
Check that the drive and motor are compatible.
Go into 1.4 Motor control menu.
Set Automatic autotuning to no if every power up autotuning is not desired.

Schneider Electric Saudi Arabia