{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the break down of list of last fault (LFT) communication network code numbers for the ATV61 and ATV71 drives.

Article available in these languages: Spanish

Issue:
Where can I find a list of last fault network code numbers for the ATV61 and ATV71 drives?

Product Line:
Altivar ATV61 and ATV71 with a network card installed.

Environment:
All

Cause:
They are using a network to read the last fault which shows up as a numerical code.  They need to convert the numerical code into a fault code.

Resolution:
See the attached document which shows the Last fault list codes.

Schneider Electric Saudi Arabia

Attachment(s)
last fault network codes.pdf [72.24 KB]