{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What terminals are a braking resistor connected to on the ATV61/71 drives?
Issue:
Braking resistor terminals connected to on the ATV61/71 drives.

Product Line:
Altivar 61, Altivar 71

Environment:
All ATV61's and ATV71's up to Frame size 12

Cause:
N/A

Resolution:
A braking resistor should be connected to terminals PA+ and PB on all VFDs up to frame size 12. Frame sizes 13 and higher require a brake transistor.

Schneider Electric Saudi Arabia