Search FAQs
What are the M221 serial port baud rate settings?
Issue:
What are the available baud rate settings for the serial port on the M221 controllers?
Product Line:
M221
Environment:
Ecostruxure Machine Expert Basic ( formally SoMachine Basic).
Cause:
Need to know what the available baud rate settings are for the M221.
Resolution:
The M221 supports the following baud rates.
1200
2400
4800
9600
19200
38400
57600
115200
What are the available baud rate settings for the serial port on the M221 controllers?
Product Line:
M221
Environment:
Ecostruxure Machine Expert Basic ( formally SoMachine Basic).
Cause:
Need to know what the available baud rate settings are for the M221.
Resolution:
The M221 supports the following baud rates.
1200
2400
4800
9600
19200
38400
57600
115200
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: