Search FAQs
Failed to Connect to the SEPAM front face using the USB cable.
Issue
When trying to connect to the SEPAM using SFT2841 with the mini USB to USB (CCA784) it fails.
Product Line
SFT2841
Environment
Windows computer management
Cause
The driver for windows is not get install or cannot find it.
Resolution
Attached are the work around for the XP and Windows 7 operating systems. If one as Windows 7 or above follow the Windows 7 pdf.
When trying to connect to the SEPAM using SFT2841 with the mini USB to USB (CCA784) it fails.
Product Line
SFT2841
Environment
Windows computer management
Cause
The driver for windows is not get install or cannot find it.
Resolution
Attached are the work around for the XP and Windows 7 operating systems. If one as Windows 7 or above follow the Windows 7 pdf.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Product:
Range:
Explore more
Product:
Range: