Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there any restriction to the cabling of BMENOC0301 and BMENOC0311 in a standalone system
When the Ethernet backplane port of BMENOC0301 or BMENOC0311 is enabled, the NOC is directly connected to the CPU. The backplane port is not protected by RSTP, Only ports 2 and 3 are protected. Connecting the NOC and the CPU via an external cable may create an unhandled network loop that may impact network communications. Refers to the User Documentation for more details

When the BMENOC's Ethernet backplane port is enabled, do not make any connections between the NOC and the CPU via an external Ethernet cable.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre