{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Smart-UPS VT-G3500; Load does not turn on automatically after an outage/shutdown


Issue:
Load does not turn on automatically after an outage/shutdown


Product line:
Smart-UPS VT-Galaxy 3500


Environment:
All Product models, all serial numbers


Cause:
The system is set to not auto start by default


Resolution:
You can set the load to turn on automatically after an outage from the PowerView display.

1. Go to Setup menu
2: Select System
3: Select Auto Start
4. Change value to On

This may take one reboot of the UPS to take affect, and you will need to turn on the load manually then.  After that first reboot it should automatically turn on in the future.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: